User Activity

If I leave all of the PullUp and PullDown pins disconnected does it matter if the USB Connector side data lines connect to D+/D- OUT while the Controller side data lines connect to D+/D- IN?This would be the opposite of what is shown in the datasheet...
Posted on January 23, 2018 at 23:47&sharpdefine TIM1_PSCRH (*(volatile uint8_t *)0x5260)I understand that now when I set TIM1_PSCRH = <some 8 bit value> that the Timer 1 Prescaler High Byte register will be set because it is located at address 0x526...
Posted on May 10, 2017 at 21:29Hello,My team and I are designing a product using the STM8S003F3. We connect to a host controller using SPI. This works great!Now I want to enable firmware update functionality. I started to get into SWIM protocol when...