Turns out error -80 is:EAUTH (80) Authentication error!"A certificate or image could not be authenticated when Trusted board boot is enabled"So we did a quick build turning this TRUSTED_BOARD_BOOT := 1to 0. But it did not work, so we’re doing a full...
We made our first breakthrough. Not there yet, but much better.We did not have the Hash and RNG (random number generated) in the device tree enabled. by enabling that, we get much further. It is very frustrating there is no error message or anythin...
@Community member Last night we traced the output on the I2C and the driver is clearly talking coherently to the PMIC:There is no reason why it is stopping after just the BUCK1 test. It conforms to the configuration file requirements, so that test ...