Was this issue solved?I have the same issue with STM32G030K6.My situation is :While the ADC input signals using Voltage divider resistance, it works correct !But if the input signals using opamp, it goes to zero ! (ADC_IN0-PA0/ ADC_IN1-PA1)I've check...