Posted on April 21, 2017 at 02:43 Hello ST community,sorry,maybe I should post my problem here. Now I am working on the wifi module X-NUCLEO-IDW01M1 ,I found some problem. Hardware:NUCLEO-F401RE,X-NUCLEO-IDW01M1 Software:STM32CubeExp...
Posted on April 20, 2017 at 04:58Hello ST communityNow I am working on the wifi module X-NUCLEO-IDW01M1,I found some problem.Hardware:NUCLEO-F401RE,X-NUCLEO-IDW01M1Software :STM32CubeExpansion_WIFI1_V3.0.1IDE: iar arm 7.70.1From the example project ...
Posted on June 06, 2017 at 14:51 Gallucci.Gerardo Das.Mridupawan Thanks a lot for your help. The board is OK now, the FAE help me update the firmware of the WIFI module. It work fine now,
Posted on May 01, 2017 at 08:39 Thanks a lot for your reply. Sorry I got the wrong connection,I monitor the RESET line and PA13 of the F401RE. Today I test it again GPIO10 is high at first,after I enter the SSID, password, encryption,then it ...
Posted on April 30, 2017 at 16:43Hi, I just connect the GPIOs 10 or 13 or 14 to the oscilloscope GPIO 10 ->keep lowGPIO 13 ->high and frames on it GPIO 14 ->high.Is this right?I connect to the CN7 of the WIFI module.GPIO 10(NC),GPIO 13(PA13),GPIO 1...
Posted on April 29, 2017 at 15:55Thank you very much for your reply.I do not have UART2USB device.I use the mbed example get nothing from the RX (PA10 F401RE) line but almost 400ms frames on the TX(PA9 F401RE) line.You suggest me to monitor the G...
Posted on April 29, 2017 at 14:34Hi Robert,Thanks a lot for your suggestion,I try the mbed example but still not work,I use the oscilloscope to monitor the RX and TX lines and find nothing receive from the RX line.Maybe the WIFI module is broken.