cancel
Showing results for 
Search instead for 
Did you mean: 

Problem with the stm32cubeExpansion wifi demo with the x-cube-wifi1

kerry liu
Associate II
Posted on April 20, 2017 at 04:58

Hello ST community

Now I am working on the wifi module 

X-NUCLEO-IDW01M1

,I found some problem.

Hardware

:NUCLEO-F401RE,X-NUCLEO-IDW01M1

Software

 :STM32CubeExpansion_WIFI1_V3.0.1

IDE

: iar arm 7.70.1

From the example project  I found two types one is SPWF01 another is SPWF04, I found the example Binary is the SPW04.

I change the config to SPWF01,but it still not work.

1)en.x-cube-wifi1_firmware (1)\STM32CubeExpansion_WIFI1_V3.0.1\Projects\Multi\Applications\

WiFi_VCOM

From the Tera term I found the print message,but when I input 'AT+S.STS',nothing output.

2)en.x-cube-wifi1_firmware (1)\STM32CubeExpansion_WIFI1_V3.0.1\Projects\Multi\Applications\HTTP_Request

From this example it will always run at the wifi init.

 file

 wifi_module.c line 294 

and can not run out this function.It seems to wait for the state.

I only changed one thing in wifi_conf.h

the old one is &sharpdefine SPWF04,I change to 

 &sharpdefine SPWF01

/**********************************/

  while(IO_status_flag.WiFi_WIND_State != WiFiHWStarted)

    {

      __NOP(); //nothing to do

    }

//always in this function

/*******************************/

Is there anyone can tell me what is wrong ? Thank you very much.

#wifi-module #stm32-f #x-cube-wifi #stm32-f4-discovery
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0