Hello,I get nearly the same problem with SD card - f_mount() returns FR_NOT_READY.I created new project using Nucleo f401re with external card slot. The D0..D3 data lines and CMD line are pull-uped internally, clock for SD is 24MHz, DMA enabled, IRQ ...
Posted on April 24, 2017 at 10:44I've got the same problem with ordering the samples - I've put to the basket the LPS25HBTR and LSM303CTR and fulfilled the form. After clicking 'submit' the form saied that all is ok but the order was not put to the ...