Posted on April 26, 2017 at 18:34First I uninstalled 'Dell SupportAssist' and the problem still occurred.I then uninstalled 'Dell SupportAssistAgent' and the problem went away.I am not sure if it was the combination of uninstalling the two programs ...
Posted on April 25, 2017 at 17:20I tried that yesterday. I removed iaStorF from the registry. Verified it was not listed in the driver. Rebooted the PC. And the problem still occurred.EDIT:Because this is the last message, any casual reader coul...
Posted on April 25, 2017 at 01:47Disabling the driver seems to fix the problem. However since it re-installs the driver everything I reconnect to the board, this seems to be only good for a temporary solution.
Posted on April 24, 2017 at 19:21If it helps, on one of the Dell laptops that does not have this problem, under Class lower filters, it only has the stdcfltn filter listed.
Posted on April 24, 2017 at 19:16MBED microcontroller USB Device Properties 'Details' TabProperty: Class upper filtersValue: PartMgrProperty: Class lower filtersValue: iaStorF, stdcfltn