When I enable lsm6dsl I2C as master , both lines are going to gnd. lsm6dsl_sh_master_set(&dev_ctx, PROPERTY_ENABLE);any tip on using lsm6dsl sensor hub, thanks
Hi Eleon,The dataready is generated by the slave as the sensor hub can only run at 104 Hz max with its own trigger to read external sensors.With Dataready generated at 400 Hz by the slave it did work, but when I switch to 1 Khz it fails. Yes, pull up...
The h3lis simply stops generating data ready signal. it looks like that at 1khz if h3lis200 not getting the read instruction in a synchronized pace.I tried to switch from 400 hz to 1000 hz after sensor hub Signals end of operation. A single readin...
Eleon,Thanks for your help, I have the system up and running. But I found the following:Im using the lsm6dsl as master and the h3lis200dl as slave of the lsm6 sensor hub, is the only device slaveI turned on start_config so that the DRDY signal from t...