I'm using STM32f429ZI Discovery board to run the touch LCD using LTDCI will attach Detatiled Log.Thank you.------------------------------------------------------------------------------------------------------------ error1: in touchGFX while generat...
How to code TFT LCD using STM32F429 any specific driver(like ST7292, ILI9341, SSD1963 etc. ) should be used in a LCD or without driver , It is possible .using touch GFX I can code any TFT LCD
I'm using STM32F429ZI discovery board and run the touchGFX template program but this show the errorI install the ST-LINK Utilities============================================================= Flash make -f ../gcc/Makefile flash Reading Touch...
STM32CubeProgrammer v2.5.0-RC1 V2.5.0 doesn't support for STM32F4 . for this please check the STM32CubeProgrammer document .So, download the STMCube IDE (v 1.1.0 )STMicroelectronics ST-LINK GDB server. Version 5.3.2Copyright (c) 2019, STMicroelectron...