Oh well ... this is disappointing. I managed to flash 'STM32CubeDemo_STM32769I-DISCO_V1.4.0.hex' according to (zip) [32F769IDISCOVERY_demo]/readme.txt. However, it ain't not the same SW that the board came with. Before the reflashing there where a 'E...
@Mike_ST >> Please don't ask why they have different size, I don't know.... and different names Which leads to the question: what is the difference between them and which one is the one to flash onto STM32769I-DISCO?
To be honest, I haven't even tried it yet J I’m planning on returning the board – and I would like to return it in its original state. The original state is demo V.1.2.0 … unless I can’t find this version I’m not even going to start experimenting wit...
I'm having the exact same question!! Thanks for 'not being alone' with that. However, I have yet another question: the hex-file from the demo is 'STM32769I-DISCO_DEMO_V1.0.0_FULL.hex'. It has version# 1.0.0 in it's name and the file is from 2018. The...