User Activity

Where can I find a list/table/docs on alternate functions for each pin ??(Not using STM32CubeMX)
Is it possible to Load/Start the Cortex-M4 from TF-A or uboot ?For our use case we want RTOS in Cortex-M4 running as soon as possible.Well before linux finishes booting.
We have a STM32MP1 system with no flash media.How do I push a TF-A/uboot image to DRAM and boot/run from DRAM withno MMC/flash media ?
Posted on September 23, 2014 at 15:46I am using UDE 4.2.05 with the SPC560B-DIS (which has UDE debug hardware built in) I can load and run code via JTAG but ... How do I access the serial port connection to the target device ??? The target microcon...
Posted on September 23, 2014 at 15:43What is the max SPC56 (SPC560B54L3) UART baud rate ? Thanks,   Stuart
Kudos from