User Activity

Hi guys,I want to develop a project, for which needs a display, and i chose the TouchGFX way. I'm using the STM32H747 microcontroller. In TouchGFX exists demos for STM32H747I Disco board, but my application will run on a custom designed board.So I tr...
Posted on October 06, 2017 at 15:49Hello,   I'm working on a project, where I need RF transceivers. I chose Your SP1ML transceiver modules, but I was dissapointed when I tried the devices, because the low distance range. The distance range abaout 20...
Posted on August 24, 2017 at 11:00Hello,   I'm working on a project where I need to shut down my device, when it finished it's task. I use an STM32L443 microcontroller to control the device. The circuit was designed, that if happens a falling edge o...
Posted on August 04, 2017 at 10:01Hello everyone,I'm working on a project, where I need to store datas on an SD card. I use an STM32L443 microcontroller. The controller communicate with another device through UART communication, and save the datas t...
Posted on February 13, 2017 at 09:43Hello everybody,I'm working on a webserver application, and I use the lwip 1.4  tcp/ip stack generated from the Cube Mx older version. Unfortunatelly I don't remember which version of Cube Mx because it was a long...
Kudos given to