User Activity

Adding DCMI to CM7 in MX (within cubeIDE) to a TouchGFX generated project against a 747_DISCO board causes stm32h7xx_hal_conf.h etc to be suitably updated, but stm32h7xx_hal_dcmi.c isn't added to build list. Is there a manual way to add this to the p...
Had to redesign my STM32F769 design take the STM32H747 (silicon supply issues). So I cloned the H747_DISCO pin for pin with the exception that I've no external Flash. I then built a TouchGFX test app based on the H747_DISCO, removed the QSPI need in ...