@Community member Yes i have found the same issue. the CLI works fine under wayland.I have found a workaround:In the in the "STM32CubeProgrammer.desktop" file located in "~/.local/share/applications"Prepend the "Exec" line with "env GDK_BACKEND=x11...
Posted on March 02, 2018 at 04:38It looks as if the STM32CubeProgrammer was written to look for libusb style drivers.This is a problem that ST should resolve with an update to the program.However you are able to get it working pretty easily.I have f...
Posted on June 20, 2017 at 05:04Hi Ari,It looks like the ADC hardware is different. From the STM32H7753xI data sheet (http://www.st.com/resource/en/data_brief/stm32h753xi.pdf)'3× ADCs with 16-bit max. resolution (14 bits 2.7 MSPS, 16 bits 168 kSPS)'...
Posted on February 15, 2017 at 23:10 Hi , Thanks for your response. Its good to hear you have also reported this issue internally. The changes for SPLIT transaction are spread across following files: Drivers\STM32F7xx_HAL_Driver\Inc\stm32f7xx...
Posted on February 14, 2017 at 22:26 I also am having trouble with this issue at the moment. st.mcu, vera.laurent, Is there anyone from ST, specifically the USB division that could look into this?