Posted on August 31, 2016 at 11:52Hello, I am currently working on a project to communicate with a Bluetooth module (BT121), to do that I use the STM32F407 eval board. Here is my configuration : // Initialize the UART3, huart3 huart3.Instance =...
Posted on September 06, 2016 at 12:15Hi, I checked everything and I still have my issue. Also Hannibal the CAN is not used in my application. If someone has some ideas feel free to share. Thanks in advance,
Posted on September 01, 2016 at 09:32Hi Hannibal, Thanks for the reply, I checked the thread and so far I think I do not have the same problem also I do not have an ''overrun error''. In my case it looks like when I have my issue the uart is in a we...