Posted on July 20, 2016 at 03:11Hi, Thanks. My colleague Adrian had a look at the c code driver and while he sees the code that queries the sensor for identity he can't see where this is used. Hope this helps. Mike Borgelt
Posted on July 15, 2016 at 02:47Hi Guys, Any progress on the problem? Are we doing something wrong with the STEVAL MKI 109V2 and STEVAL MET 001V1 combination? Once we have tested the 3 MET001V1 I have we're ready to buy a bunch of them.
Posted on July 07, 2016 at 08:53 Thanks, Antonella, Images in attached zip file. FWIW I have checked continuity between the parts at the visible pads at the device and the pins and all seems OK. Trace code on parts tested 11621012 1...
Posted on July 05, 2016 at 07:23Sorry, that should be I have a couple of STEVAL -MKI165V1 sensors. Unico is showing GUI 4.6.1.0 Beta, firmware 4.0.14 after upgrade