Posted on May 25, 2016 at 18:20Hi, I'm setting RTC for wakeup interrupt using HAL as below but the interrupt not happen. Please give me your advice. Thanks. P/s: - These codes are based on CubeMX. - Other settings required for system running is ...
Posted on May 01, 2016 at 21:43The original post was too long to process during our migration. Please click on the attachment to read the original post.
Posted on September 10, 2016 at 18:05Hi Clive1, I've had them same issue with UART IAP on STM32F3Discovery board. I use Realterm to send 0x7F, I received 0x79 as said. But in Flash Loader Demonstrator v2.8, it always says ''Unrecognized device...Ple...
Posted on May 02, 2016 at 11:22 Just for more information. I also tested with VBAT, and the return value is about 3050. On the board, VBAT is connected to VDD = VDDA = VREF+. If correctly, it must be 4095. Testing with other external channels (ADC1_...