2016-05-25 9:20 AM
Hi,
I'm setting RTC for wakeup interrupt using HAL as below but the interrupt not happen. Please give me your advice. Thanks. P/s: - These codes are based on CubeMX. - Other settings required for system running is done by CubeMX generated-code. I don't include it here. === int main(void) { // setup RTC RTC_HandleTypeDef hrtc; hrtc.Instance = RTC; hrtc.Init.HourFormat = RTC_HOURFORMAT_24; hrtc.Init.AsynchPrediv = 100; hrtc.Init.SynchPrediv = 400; hrtc.Init.OutPut = RTC_OUTPUT_DISABLE; hrtc.Init.OutPutPolarity = RTC_OUTPUT_POLARITY_HIGH; hrtc.Init.OutPutType = RTC_OUTPUT_TYPE_OPENDRAIN; HAL_RTC_Init(&hrtc) HAL_RTCEx_SetWakeUpTimer_IT(hrtc, 3, RTC_WAKEUPCLOCK_CK_SPRE_16BITS); while(1) { } } void HAL_RTC_MspInit(RTC_HandleTypeDef* hrtc) { // called by HAL_RTC_Init if(hrtc->Instance==RTC) { __HAL_RCC_RTC_ENABLE(); HAL_NVIC_SetPriority(RTC_WKUP_IRQn, 0, 0); HAL_NVIC_EnableIRQ(RTC_WKUP_IRQn); } } void RTC_WKUP_IRQHandler(void) { printf(''Wakeup Timer Interrupt\n''); HAL_RTCEx_WakeUpTimerIRQHandler(&hrtc); } === #stm32f3discovery2016-05-25 10:49 AM