I am using a STM32F412CGU6 and selected PB_9 to be the CAN Tx pin. The pin then idles at 2.8 volts. If I use it as a standard IO pin, it will go to 3.3 volts. If I assign the CAN Tx pin to PA_12 it also idles at 3.3 volts.I am using mbed 5.12
Thanks for the hint. It got me to step through the MBED/HAL initialization code and examine each configuration argument. To discover that I have been mapping the TD pin to the wrong output pin (PA_12 instead of PB_9) all the time. The configuration f...