User Activity

Posted on February 19, 2017 at 18:58Hi,I need to change sampling rate from 48kHz to 16kHz and came across SRC236 which is part of X-CUBE-AUDIO-L4 library. Unfortunately there is no source or download link avalible anywhere on ST website. I found onl...
Posted on February 15, 2017 at 09:59 Hi, I'm having toruble with configuring SAI clock. For 48kHz sampling rate I need 12,288MHz MCLK but I'm confused with settings in CubeMX clock configuration tab. To SAI2 clock to arbitrary 24MHz but what shou...
Posted on February 10, 2017 at 16:55Hi,I'm trying to communicate with http://www.analog.com/media/en/technical-documentation/data-sheets/ADAU1761.pdf via SAI, STM32L476 is master. I sucessfully connected to it via I2C, now I need to send data. I don...
Posted on May 09, 2016 at 22:33I want to use CH1 and CH2 in encoder mode and also CH3 in input capture mode, all this using one timer (TIM3). Is it possible? I didn't found any warnings in datasheet. I looked at the block diagrams but I'm not sure a...