Posted on May 18, 2016 at 14:51Thanks for the suggestion. Unfortunately, Stm support say ''There is an issue in our OTG implementation, there should be published an errata on this point long ago, but so far it is not. The problem is present on your ...
Posted on April 25, 2016 at 14:56I have done the procedures that support the hub. This works well for fs devices. I can not understand why the error by receiving / transmission channel leads to the disable of the usb port. You used to work HCC embed...
Posted on April 21, 2016 at 13:08I checked the changes in those files that I use for usb. Changed version number and also to change constant (ex., 0 -> 0U) This does not affect anything. I changed the usb core FS -> HS. Almost too. But there was...
Posted on April 20, 2016 at 08:11Hi! I have the same problem. In my request to support I received no answer I use stm32f4discovery in FS_HOST mode of HAL library V1.4.3 11-12-2015 Through FS hub is connected to the host LS mouse. The problem arises...