Hello,I got the blue board MB1075-F429I-E01I used TouchGFXdesigner 4.14.0I upgraded now to 4.16.1 , This version works now with my board, it has a different board selector and produces the right code.The compiled binary firmware file from the board s...
Hello,I investigated quite deep into this issue and my case is still open at ST.For now I also modified the code in BSP_TS_GetState.Modification y = 320 - y; I subtract the y coordinate from pixelheight to invert y.Now it works.../Oliver
Hello, I got the exact same issue with a new 429-disc1 board. Touch was working correct when the board arrived. After upload from TouchGFXdesigner the screen touch was verticaly mirrored. Example, when a button was at the top of the display I had to ...