User Activity

Namely, I want to know the linear acceleration sensitivity of the LSM9DS1 expressed in (m/s^2)/LSB, not in the g/LSB. It is well known that g at the Earth Poles is 9,832 m/s^2, but at the Equator is 9,780 m/s^2.Yes, such few difference is important f...
Posted on July 07, 2018 at 09:55I have conducted little research of temperature influence on accelerometr and gyroscope readings. The sensors were cooled to a negative temperature on celsius, and then heated under the IR lamp to approximately 50 deg...
Posted on June 18, 2018 at 13:10Hello! I have looked at video about X-CUBE-MEMS1 ( /external-link.jspa?url=https%3A%2F%2Fwww.youtube.com%2Fwatch%3Fv%3D45baO5Lxv-o%26t%3D313s ). After that, I've installed Unicleo-GUI and in tab FW Managment I don't s...
Posted on January 16, 2018 at 11:10In the datasheet say that this pin must be work(indicate moment of magnetometer new data avalaible ) automatically(without need of configuration), but it doesn't work. Why? In the http://www.st.com/resource/en/data...