can u please suggest me how do i calibrate for an accurate long range.i have tried out with ur previous suggestions but the error is more than 3% of actual distance.here is my code:#include <Wire.h>#include <VL53L0X.h>VL53L0X sensor;void setup(){ Ser...
it will be mounted to TOP OF A LARGE WATER TANK of 200,000L capacity. Since the tank is in the exteriors (exposed to Sun light), there is Humidity inside the tank in the open space between water and the sensor.What type of harm this can cause to the...