Hello, I have the Question & Answer below.(1) I use the NFC, but I don't know about the NFC forum. So, I want to know if the size of the NFC Antenna design I want is possible. (2) 0,0,40 => Ok-Point & 0,0,10 => Nok-Point --> Question : I do...
Dear ST..I am RYU, a Community Member's HW engineer.History is as follows. (From a H/W point of view...)(1) Our NFC Antenna size is different from ISO(NFC Antenna size). --> Antenna size 146mm * 86mm(Reader and Tag antenna size are the same si...