User Activity

Posted on October 21, 2015 at 14:04 I know that the HTTP file image can be downloaded from an HTTP server and written to flash using AT+S.HTTPDFSUPDATE. Could it be possible to add the capability to load the HTTP file image to flash by sending the i...
Posted on October 15, 2015 at 17:00 I've just wasted an STM32405 chip + a day of my time trying to work out why the USB FS CDC device wasn't working on a new (partially populated) board that I was testing. Why wasn't the USB working? Well, the board...
Posted on October 06, 2015 at 16:31 Next problem... I have enabled flow control on the module and the MCU and now attempting to use a bit rate of 460800. Both ends are using the right bit rate but only the MCU appears to be controlling an RTS signal...
Posted on October 01, 2015 at 09:51Hi, I am broadcasting a small UDP packet once a second through the SPWF01 using AT+S.SOCKON=192.168.1.255,55555,u and AT+S.SOCKW and that appears to work just fine but if I access the SPWF01 web server at the same...
Posted on July 27, 2015 at 16:23Hi, When the SPWF01 is in miniAP mode what setup will allow the client to resolve the module's domain name. Do I need to set ip_dns to be the module's IP address ? Thanks, Mark