User Activity

Hi,I have STM32 NUCLEO-L432KC Nucleo-32, I would like to power it from a li-pol battery. Is it possible?
Hi,I'm working on a prototype of a device. One of this device features is to collect data from gyroscope, accelerometer and e-compass. It is very important that the device will be ultra-low-power. One goal for the prototype is to verify how much ener...
Does the X-NUCLEO-LPM01A allow to measure power consumption of boards like Pi Pico, Arduino Nano Connect RP2040? Or only Nucleo boards?I have nucleo board to which i have connected GPS module, IMU, LCD display. Will the Power Shield measure power con...
Hi,So far I was using Nucleo WB55 and everything was ok with ST-LINK. Now I created new project and switched to Nucleo H723ZG. When I try to run or debug I receive message:No ST-LINK detected! Please connect ST-LINK and restart the debug session.The ...