Hi Martin,My final goal is to create an application whith multiple screens. Some screens whith a slider, more than one button in each screen and controlled only by a rotary encoder and a push button to replace the touch input. Eventualy I will have t...
Hi Scott,You can find some of the core files in Application->User in CubeIDE, there are the files generated by TouchGFX as well and you can edit the files from here. I think these are shorcuts to the actual files.Which variable are you trying to acce...
Hi WoulaI'm having the same problem, I think the best way to integrate is to create a project from TouchGFX and then in CubeIDE "File->Open Projects from File System" and select the folder "STM32CubeIDE" inside the TouchGFX's project. I don't know if...