User Activity

Posted on October 19, 2015 at 19:02 Hello, I am using the ST-Link V2 debugger to run on target unit tests. I have updated my windows drivers to the latest and the firmware on the debugger has been updated to the latest as well. Tests are...
Posted on August 29, 2014 at 19:35I am trying to setup ADC sampling that is triggered by a Timer. Essentially I want to setup a 1 kHz timer that will trigger an ADC sample every 1 ms, and use DMA to transfer the sample data. I have all the component...