Posted on May 17, 2018 at 10:03From what i can say, the LL is a newer version of the SPL, and what HAL should have been. Especially if you define FULL_LL_DRIVER (or something along those lines) you get something that looks a lot like SPL. For me, t...
Posted on April 14, 2018 at 17:29Apart from debug support (which would certainly be nice), all the reasons there are to use a decent IDE are reasons to use Eclipse instead of the Arduino, erm, environment.I am working on a prototype for which someon...
Posted on September 27, 2017 at 16:41I have no idea if it is the same problem (and i don't use the HAL if i van avoid it) but we had a problem like this using the SPL, especially when switching between transmit/receive mode. Today i ported that stu...
Posted on March 04, 2014 at 14:14Does this mean that generating a new CDC skeleton does not work yet? I have tested it now with a project based on the older USB libraries and verified that at least the hardware is ok, but the generated project from ...
Posted on March 03, 2014 at 15:35I am also having troubles generating a working USB CDC skeleton for the STMF4Discovery board : it seems there is no communication between the PC and the uC as even the device descriptor is not received by the host. H...