User Activity

Helloon the a.m. device I use both ADC1 and ADC2. The initialization is identical on both. I notice that results fluctuate widely at ADC1 output and reasonably at ADC2 output.Grounding ADC1 input leads to 330-345 LSB.Vdda = 2.5V from precise external...
HelloI wonder if there is some example code available on how to use the Data EEPROM in the 8pin STM8L001J3.I did successfully work with the internal Data EEPROM on the STM8L051, but no success on the SO8. The address I used is 0x9BFB (in contrast to ...