Hi @Martin KJELDSEN ,I can't see the startup-code anywhere in the project explorerYes, I did configure the external loader but it doesn't change anythingThanks for your help,Augustin
I generated a project with TouchGFX with the replaced .tpa template (%APPDATA%/TouchGFX-4.13.0\STM32F746G_DISCO\3.0.0 did not exist, it was under %APPDATA%/TouchGFX-4.13.0Downloads\STM32F746G_DISCO\3.0.0).Everything compiles fine but I still get the ...
The TouchGFX project generation works but I can't import it in CubeIDE.There is no error message but the project doesn't show up in the project exploreredit: I already had a projet with the default name ...
Thanks for the answer, in fact I saw an answer by @Martin KJELDSEN in this thread. He experienced the same issues and I quote him : "I have a fix for this CubeIDE debugger issue. I just forgot to upload a new template - Will get on it ASAP!".