User Activity

I was looking at STM32N6, and it says it has 1G networking. Problem is, chip used is 100M. So how can they say that development kit supports 1G ?LAN8742A-CZ-TR chip used inside both devkits:Same goes to HR timer, it says on datasheet, it does support...
Hello,Is there any chance ST could provide examples or guidance on interfacing a CSI (MIPI) camera with Raspberry Pi Camera Module 2 NoIR cameras?From my initial research, it seems the CSI connector uses the same pin layout as Raspberry Pi cameras. H...
Hello,I am developing project where I need to do some image processing on BW image. All was great, but I started having problems with DMA (maybe I always had, don't recall)Idea is that I simply load data to internal SRAM with DMA, and when I get TC, ...
Hello,In my project I need to sample 3 phase current to see if where is short or not. I am using STM32H753 HRTIM. Not only that I must place sampling point as close to PWM transition from high to low as possible (peak current)I connected phase curren...
Hello,In my project I need to have ~25KHz high resolution PWM generation. So for this I selected STM32H753 with 480MHz HRTIM1.I am struggling producing correct outputs for my needs, maybe some one has this done already and care to share the project ?...
Kudos from
Kudos given to