@TSerr.1 When I read "M-sequence Capability" (0x03), it return a value of '0'. So I thought that other types other than TYPE_0 is not supported. After I look more carefully into the IO-Link specs, I see that this is not the case. And your point of ...
@TSerr.1 Thanks for reply. My device does not support Type 1 and Type 2. Only Type 0 is supported.I have tried writing to "MasterCycleTime" but the value in it is not updated when I read it. However, when I write to "Direct Parameter Page 2" which c...
Yes. I can read MinCycleTime but unable to write to MasterCycleTime.I believe you have not entered into OPERATE mode as the cyclic data exchange is not started.Have you tried writing the value "0x99" to address "0x00" (MasterCommand)?
Sorry. I made a mistake there. Yes, it is "Diagnosis" but it still doesn't work for me. Do I have to switch it OPERATE before this can work?But I am having a hard time writing to the sensor. I tried writing to "MasterCycleTime" which is both readable...
@LHaim This does not work for me as "dataBuffer[0] = 0xCA" has the "Comm Channel" set to "ISDU" and my device does not support "ISDU".Thanks a lot for your help. I will see if I can come across the information to set up the device cyclically and wil...