Yes, that would be an option. but you could also push it back to t = 0. The plot of the array would then be delayed by half a second compared to the real time graph. I want to see values of an array in a time plot, my screenshot only displays one pos...
For my situation: Create a new "variables" node. Add the whole array and set in the "Acquisition paramters" = Sampling frequency e.g. 2Hz. (For me it means, that the array will be read out every 500ms). On the "chart" the data values in the array wil...
I have the same question! I want to plot an array with [21000] uint16_t audio datas, comming from a mic. into ADC. The array is refreshed (or filled) every 500ms via DMA. So it is 42kHz Sampling rate. When i tried to pick the right buffer in the CUBE...