User Activity

I am struggling to get an STM32G070RBT6 into bootload mode with the boot pin.Using ST-Link utility I have set nBOOT1 = 1, NBOOT_SEL = 0 and left nBOOT0 = 1.If I have understood the datasheet correctly this should allow me to enter bootload mode by ho...
Posted on May 02, 2018 at 12:36I am posting data up to a server using HTTP post, the module sends the data in chunked mode. It is a relatively short packet, so is sent in one transfer. However the module does not end the transfer by sending a last c...
Kudos from