Hello community,i want to know what’s the difference between the adv7533 that sits in the F7 Cube and the H7 Cube? Why there are extra files for the H7 Cube? (reg.h and reg.c)thank you
hello ST community,I'm wondering why when I'm touching the screen (interruption) the screen refresh twice and when I do this with a push button (interruption too) it refreshes only once. is there an explanation for that (I want that the display refre...
Hello @Community member ,i got this screen, I, now, wonder why the FPS start with 3.5 and drops to 0.2, and also there’s no image on the screen, how could solve this?
i got this whole project from the H747I application, it seems to be working on it even there’s no source file for ai_platform_network_process, here I joined a pic, I got a screen tears then a HardFault is raised
I think, because that function doesn't have a definition, it's only in a .h file, but I saw that there's a lib folder which contains :NetworkRuntime512_CM7_GCC.a, I think there's something there to link with it. It's like a .dll, linking at runtime.