User Activity

Hello,I have second stage bootloader in place and want to change RDP level from it (0 to 1 and roll back when doing firmware upgrade).However, the problem is, once RDP level is changed to 1, bootloader is not able to change it back to 0. I've to chan...
Hello All,I am working on a system and my firmware consists of a boot-loader (Second-Stage Boot Loader) and application. Boot-loader is occupying sector 0-3 and Application lies in sector 4 to sector 11 of micro-controller flash (STM32F767).Problem s...
I'm using I2C2 engine of the STM32F767ZI MCU on PF0 & PF1 pins as master to communicate with 4 slaves at 75khz. The operation is not using Interrupt on tx/rx or DMA and with FreeRTOS environmentSCL and SDA are pulled up on board with 4.99K.The pollin...
Kudos from