User Activity

Hello, I am investigating if I could include a register value in the NDEF field.My goal is quite simple, check value of register 5 tamper configuration and report it via NDEF so it a user could scan the tag on their iPhone and send and SMS with the t...
Posted on April 06, 2018 at 17:10Hi There,I am going a bit crazy about this. I have a custom board with STM32412 on it. I have connected TX and RX to PA9 and PA10, I ensure that Boot0 == 1 and PB2 (boot1) == 0 (just in case). As per  AN2606.And the ...