h7b0, had some feedback for st support but with some specifics vaule could be use to generate firmware, but the recommendations is still to add external flash/ram
Most of this things i think are good for boards that touchgfx already give us a template, but for a mcu that doen't is on the touchgfx will be differente using the cubeID interface, now one of my main problems is that is consumes so much ram and flas...
Hello, i have the same doubt, so the only way to begin in a custom board/tftLCD is via CUBEID ???i was also wondering if i could start a project with touchgfx and then import it to cubeID, but do not know how to relate it with a specific mcu.Doing it...