User Activity

I am working with Murata community but thought I would also see if anyone has experience on our specific type of board. Our design is based on STM32MP175C. They mention needing custom FW and their Yocto layer, etc. Seems emphasized on working with N...
This is an STM32MP157c based board design with Micrel KSZ9021GN PHY in 100 MII mode. Have you ever seen this situation before? Here are the relevant parts of the boot, the early kernel part looks normal and the LEDs are on.... [ 2.507568] stm32-dw...
Same situation as before - using a STM32MP157C based design + KSZ9021GN PHY but now actually wired for MII mode. Previous board was wired for GMII mode, even verified by Microchip/Micrel, not realizing the MPU did not support that mode (should have c...
OpenStLinux 5.4 Dunfell 06 22 20 Boot chain of TF-A, U-Boot and kernel. I had forked the three .dts files with custom board names. TF-A starts fine.But in u-boot, hangs before it starts. With exact same dts contents just using original dts name as t...
Not sure if this is the best forum for this question but I am using the USB OTG port in device mode as ethernet gadget. It works fine if plugged in from boot, or first plug in anytime after. But if unplugged and plugged in again it will not come back...
Kudos from