That is the way I'm sending out the Data:for (uint8_t c = 0; c < txBytesToSend; c++)
{
USART2->DR = tx_Buffer[c]; // Load the Data
while (!(USART2->SR & (1<<6)));
}Between the read and the write operations there are no delays inside which cou...
Hello Tesla!I am using the HAL_Transmit Function to write exactly the length I am writing to the function. My question is, why does the Modbus Master is receiving less bytes than Hterm. It looks o.k. on Hterm.
I just wrote a basic modbus slave on the STM32F401RE.I am using a Baudrate of 19200 (tested also with 9600) and with the terminal "hterm" everything is working fine. As you can see in the picture below... I am getting the right frame with its correct...