Hello! I noticed a speed error on MCU L476 and L433. When setting MSI frequency to 1 MHz, the frequency is 1015.5. (Auto trimered by LSE, LSE enabled and work well) At higher frequencies, the operation is normal. What could be the reason?
Yes, but in erratasheet not fixed.I would like to work at low frequencies with quartz stability. But HSE quartz consumes a lot of energy (above 1mA)... It seems that you will have to work at a frequency above 2 MHz
1MHz is always off 1.5%, good temperature stability. When I turn off the LSE, the frequency is 998 kHz and is very temperature dependentRCC_CR.MSIPLLEN SET_BIT(RCC->CR, RCC_CR_MSIPLLEN) ;
at lower frequencies below 1Mhz MSI get wrong freq, wen i set freq abowe 1 MHz MSI work well.LSE actually running.I see this in the care of the frequency when heating and cooling the chip. Indeed, auto-tuning works excellently. When I turn off the MS...