User Activity

I am trying to debug some proof of concept code on a STM32F746 Discovery but STM32CubeIDE throws a "No ST-LINK detected" error. However the STM32CubeProgrammer can access it fine after the firmware on the ST-Link part of the board was updated.I have...
I have started from the command line so I can see errors. It starts up ok but when I try to create a new project using "ACCESS TO MCU SELECTOR" it throws the error:Exception in thread "AWT-EventQueue-0" java.lang.NoSuchMethodError: com.st.microxplor...
I have a new PC so was trying to install STMCUFinder. It does not like the version of Java I have, OpenJDK 11.0.3. The problem is very recently Oracle have withdrawn their freely downloadable versions of Java so you now have to enter into an agreem...
I have a product deployed in the field that uses the STM32F030CCT. Due to time constrains it was shipped without a boot loader but I was able to put in a bootstrap that allows me to load code to RAM and run it. I now need to do that but I have foun...
Posted on February 22, 2018 at 21:09I have just installed the new STM32CubeProgrammer for Linux but it won't run. I see the error 'Error: Could not find or load main class com.st.app.Main'. Anyone else come across this problem that has a fix?I went ...
Kudos from