Hi,
There is no Ux_Device_MSC examples in x-cube-azrtos-wb/g4.
All MSC available examples run on OTG_HS capable platforms such as h7.
I have tried to port one example to STM32WB55 but face issue with it (more information at the bottom of the post...
Nice one. As mentionned there are multiple ways to provide 3.3V but my prefereed one when using a segger J-Link is by getting it from the probe itself (5V supply) to the Nucleo VIN sparing a USB cable. The only thing needed is a "Target.PowerOn (BP_S...