User Activity

if anyone already done or any example demos please share,i have a working webserver with static webpage , need to create a dynamic webpage with user login .if any demos or references kindly give link .thanks in advance.
hi i am using cubemx and generated an ethernet webserver project from example on nucleo f429i board it is working with default webserver page. However i need to use my own custom webpage , but do not know how to generate static webpage i followed som...
The problem is crc used in iap for transferring the bin file is to only check for errors during the transfer process , however i dont want any random bin files to be flashed into the flash or executed from it, only certain signed bin files need...
The nucleo ported project doesn't work , i cant understand what could be the issue . I keep getting verification failed error , HAL_TIMEOUT .The download timeout is 10000U ,changes made to it (50 seconds) how does this impact the code, will it wai...
Kudos from