Posted on January 24, 2018 at 09:37im lost! im trying to create usb cdc in STM32F405RGthe only thing im doing is to configure usb_fs as device and the usb class as a communication device class than i generate a code in STM32CUBEMx when using STM32L4...
Posted on January 21, 2018 at 19:10hi every one, i am using STM32CUBE with STM32F4 processor and i want to send small amout of data through USB but it takes a long time using the CUBE function USB_CDC_TRANSMIT. can someone help me do, thanks!