User Activity

Can someone please point me at a document that identifies any changes in the STM32H743 between the original 400MHz capable version and the latest 480MHz versionThanks
I'm running a USB keyboard on an H743. This works completely reliably at all CPU speeds up to and including 400MHz. However, above 400 MHz the connection is no longer reliable. Sometimes the keyboard connects perfectly and then it will work properly ...
The clock and data lines on SPI seem to go tri-state off when not in use even though the SPI channel is left open. Is this expected behaviour? It causes issues with some connected chips as they see the re-establishment of the driven clock signal as a...
I'm still having problems with VBAT current consumption. I've loaded my firmware and the processor behaves correctly in all other respects. I removed all components from the processor to insure that there are no sneak paths for parasitic current dra...
I'm toggling an I/O in the SYSTICK interrupt every 0.5 seconds with the processor running at 168MHz and using an RTC interrupt to wake the CPU from sleep. This all works well and the processor wakes up after the programmed interval. As per the HAL ...
Kudos from