I'm using the STM32F072B-DISCO, trying to implement an example code for the touch sensing and followed the instructions of the "Getting Started with touch sensing Control on STM32 MCU". The code given in chapter 7.3.6 results in errors. see belowone ...
On Page 8 Chapter 4 Electrical Characteristics, the Value IIN says on Shutdown mode with RPRG = 24kOhm is typically 60uA. This is quite a lot! Does this current also flow when the charging adapter is not connected anymore, meaning Vin = 0V ?