When I use the VL53L1X API the optical center is filled in by using the ROI center. If I then run with the VL53L1 API I get a values read from the device that have the fraction filled in. They are close to 8. What do these fractional values mean? X =...
What is the expected value if the device were to be manufactured perfectly? What is it if the optical center is actually half of a SPAD low and to the left at the center of the block marked 7, 7 in the user manual?ThanksBoB